About the maximum capacity of ECSPI of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the maximum capacity of ECSPI of i.MX6Solo

Jump to solution
668 Views
yuuki
Senior Contributor II

Dear All,

Would you teach the maximum capacity which ECSPI of i.MX6Solo supports?

We want to connect SPI-NOR Flash of 512Mbit to eCSPI.
We want to know whether eCSPI of MX6Solo will support this.

Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
1 Solution
562 Views
Yuri
NXP Employee
NXP Employee

   Usually SPI NOR is used for boot : the ECSPI can read data from EEPROM using 2 or 3 byte addressing.

Three byte addressing means 16 MB.


Have a great day,
Yuri
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
563 Views
Yuri
NXP Employee
NXP Employee

   Usually SPI NOR is used for boot : the ECSPI can read data from EEPROM using 2 or 3 byte addressing.

Three byte addressing means 16 MB.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos