About the maximum capacity of ECSPI of i.MX6Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the maximum capacity of ECSPI of i.MX6Solo

ソリューションへジャンプ
1,425件の閲覧回数
yuuki
Senior Contributor II

Dear All,

Would you teach the maximum capacity which ECSPI of i.MX6Solo supports?

We want to connect SPI-NOR Flash of 512Mbit to eCSPI.
We want to know whether eCSPI of MX6Solo will support this.

Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,319件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Usually SPI NOR is used for boot : the ECSPI can read data from EEPROM using 2 or 3 byte addressing.

Three byte addressing means 16 MB.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,320件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Usually SPI NOR is used for boot : the ECSPI can read data from EEPROM using 2 or 3 byte addressing.

Three byte addressing means 16 MB.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信