About the function of the FEC driver of Linux BSP for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the function of the FEC driver of Linux BSP for i.MX6

963 Views
yuuki
Senior Contributor II

Dear all,

We use i.MX6DL by our system.
OS is Linux L3.0.53 (Based on NXP BSP)

We have a question about FEC driver included in L3 .0.53 BSP

<Question>
We want to use Loop back function of the Etnernet PHY.
Is Loop back function included in FEC driver?

KSZ8091RNA is used as Ethernet PHY.

Ether_PHY_LOOPBACK.png

Please refer to section "3.7.1 LOCAL (DIGITAL) LOOPBACK" of the attached file.


We want to confirm whether transmission data match with reception data by using this function.

May I have advice?

Labels (3)
0 Kudos
1 Reply

729 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

for internal loopback nxp fec driver please refer to

internal loopback test for freescale fec driver on i.MX6 platform 

As KSZ8091RNA is not used in nxp bsps (AR8031 is used on i.MX6DL Sabre board),

I am afraid such loop back function for that etnernet phy is not available.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos