About the device which supports MLB in i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the device which supports MLB in i.MX6

ソリューションへジャンプ
2,243件の閲覧回数
george
Senior Contributor II

Dear all,

I received the question about MLB from my customer.

In my understanding, only the product of the automotive grade is supporting MLB.

However, in i.MX 6Solo/6DualLite datasheet for Consumer Products, these are described as one of the functions of all devices.

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf#page=3

Are these incorrect?

Best Regards,

George

ラベル(5)
0 件の賞賛
返信
1 解決策
1,751件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The Table 1 is not fully correct.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,751件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please use part number coding (part differentiator field) to define
what parts support the MLB. Please look at Figure 1 (Part Number
Nomenclature) of the i.MX6 Datasheets. Say, number 7 for i.MX6 D/Q
means :
“Industrial – w/ VPU, GPU, no MLB”.

The i.MX6 Series Datasheets :
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQAEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLIEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


0 件の賞賛
返信
1,751件の閲覧回数
george
Senior Contributor II

Dear Yuri,

That is, are Example Orderable Part Numbers Options field in Table-1 wrong?

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best Regards,

George

0 件の賞賛
返信
1,752件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The Table 1 is not fully correct.

Regards,

Yuri.

0 件の賞賛
返信