About the device information which can be connected to USCAR_TYPE_A for SABRE-AI_Base Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the device information which can be connected to USCAR_TYPE_A for SABRE-AI_Base Board

424 Views
yuuki
Senior Contributor II

Dear all,

We want to try that we input LVDS signal into USCAR_TYPE_A(J37: Rear Camera) of SABRE-AI_Base Board

Is there any information of the Camera or Device which can be connected to this USCAR_TYPE_A?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Reply

312 Views
art
NXP Employee
NXP Employee

The LVDS de-serializer, used on this input, is DS90UR124QVS by Texas Instruments. It supports the FPD-Link II compatible input. So, any device that provides the FPD-Link II output, can be connected there.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos