About the VSNVSVOLT default value for PF0100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the VSNVSVOLT default value for PF0100

跳至解决方案
1,176 次查看
yuuki
Senior Contributor II

Dear All,

We referred to the following part.

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
- Table 109. Register VSNVSCTL - ADDR 0x6B (P.110)

According to this, the VSNVSVOLT field is 3bit.
However, this default value is 0x80.

We think a description of the default value is mistake.

Would you confirm this?

Best Regards,
Yuuki

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,111 次查看
art
NXP Employee
NXP Employee

Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,112 次查看
art
NXP Employee
NXP Employee

Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复