Dear all,
We use i.MX6Solo and PF0100F0AEP.
I seem that a spec of the VSNVS output of PMIC do not match a spec of VDD_SNVS_IN.
I think that the Min value of VSNVS is less than the Min value of VDD_SNVS_IN.
Does this affect the operation of i.MX6solo?
Or, Is it the mistake of specifications of which?
For VDD_SNVS_IN of i.MX6Solo,
According to the "Table 8 Operating Ranges" in Datasheet, it is defined at 2.9V - 3.3V.

However, for VSNVS of PF0100,
According to the "Table 111. VSNVS electrical characteristics" in Datasheet, it is defined in 3.0V +/-5.0%.
So, the voltage range is from 2.85V to 3.15V.

May I have an advice?
Best Regards,
Yuuki