About the Absolute Maximum Ratings Value for i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the Absolute Maximum Ratings Value for i.MX6Solo

476 Views
yuuki
Senior Contributor II

Dear all,


We have a question about Absolute Maximum Ratings for i.MX6Solo.


We found a difference between Rev5 and Rev6 of Datasheet.

For IMX6SDLCEC Rev. 5, 06/2015,
 - VDD_ARM_IN Max value is 1.5V.
 - VDD_ARM_CAP Max value is 1.3V.

Rev5_Absolute_Maximum_Ratinges.png

For IMX6SDLCEC Rev. 6, 08/2016,
 - VDD_ARM_IN Max value is 1.6V. (LDO enabled)
 - VDD_ARM_CAP Max value is 1.4V. (LDO enabled)

Rev6_Absolute_Maximum_Ratinges.png


Would you tell me the reason why these values were changed to?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Reply

393 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 7 (Revision History) of the Datasheet IMX6SDLCEC Rev. 6, 08/2016 :

"All maximum voltages increased (improved)." This is result of more careful testing.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos