About setting of the EIM timing.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About setting of the EIM timing.

跳至解决方案
1,121 次查看
tomo
Contributor II

Hi,

Now I considering EIM timing parameter to set to WCSA=2, WEA=1 for asynchronous memory access.
Does i.MX6D accept this setting and properly work ?

Best regards,

标签 (1)
0 项奖励
回复
1 解答
1,061 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  generally it is possible to set to WCSA=2, WEA=1 for EIM asynchronous memory access,

but exact configuration depends on application. Use specs of the device, connected to the EIM.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,062 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  generally it is possible to set to WCSA=2, WEA=1 for EIM asynchronous memory access,

but exact configuration depends on application. Use specs of the device, connected to the EIM.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复