About setting of the EIM timing.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About setting of the EIM timing.

Jump to solution
466 Views
tomo
Contributor II

Hi,

Now I considering EIM timing parameter to set to WCSA=2, WEA=1 for asynchronous memory access.
Does i.MX6D accept this setting and properly work ?

Best regards,

Labels (1)
0 Kudos
1 Solution
406 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  generally it is possible to set to WCSA=2, WEA=1 for EIM asynchronous memory access,

but exact configuration depends on application. Use specs of the device, connected to the EIM.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
1 Reply
407 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  generally it is possible to set to WCSA=2, WEA=1 for EIM asynchronous memory access,

but exact configuration depends on application. Use specs of the device, connected to the EIM.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos