Dear all,
I investigate DVFS function of i.MX6UL.
In AN5170, The voltage levels of VDDARM and VDDSOC is shown in following Table1.
On the other hand, in i.MX Linux Reference Manual for i.MX6UL,
Dynamic Bus Frequency Driver has three set points.
- 1. High Frequency Setpoint
- 2. Audio Playback setpoint
- 3. Low Frequency setpoint
Does the table1 of AN5170 match those set points of Dynamic Bus Frequency Driver?
For example,
When High Frequency Setpoint is set, the voltage of VDDSOC and VDDARM in 528MHz is used.
May I have advice?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi Yuuki
voltage levels of VDDARM and VDDSOC affect cpu frequency - CPU Frequency
Scaling (CPUFREQ) Driver and does not affect Bus Frequency Driver
(it varies the AHB/DDR frequency).
CPU Frequency Scaling (CPUFREQ) Driver and Bus Frequency Driver are different drivers.
For Dynamic Bus Frequency Driver frequency values one can look at (attached)
linux-2.6-imx-imx_3.14.38_6ul_ga/include/linux/busfreq-imx.h and
Linux/Dcoumentation/...arm/imx/busfreq-imx.txt
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuuki
voltage levels of VDDARM and VDDSOC affect cpu frequency - CPU Frequency
Scaling (CPUFREQ) Driver and does not affect Bus Frequency Driver
(it varies the AHB/DDR frequency).
CPU Frequency Scaling (CPUFREQ) Driver and Bus Frequency Driver are different drivers.
For Dynamic Bus Frequency Driver frequency values one can look at (attached)
linux-2.6-imx-imx_3.14.38_6ul_ga/include/linux/busfreq-imx.h and
Linux/Dcoumentation/...arm/imx/busfreq-imx.txt
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------