Hello,
The following is described outside the table of Table 5-5 of the reference manual.
Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?
2.Automatic enter self-refresh when there is no DRAM access.
best regards
Goto
解決済! 解決策の投稿を見る。
Hi goto11
>Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?
yes this can be implemented by programming REFRESH_TO_X32 field register DDRC_RFSHCTL0
described in sect.9.2.4.5.2 Refresh using auto refresh feature inside the DDRMC
i.MX 7Dual Applications Processor Reference Manual
Best regards
igor
Hi goto11
>Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?
yes this can be implemented by programming REFRESH_TO_X32 field register DDRC_RFSHCTL0
described in sect.9.2.4.5.2 Refresh using auto refresh feature inside the DDRMC
i.MX 7Dual Applications Processor Reference Manual
Best regards
igor