About self-refresh of DRAM (LPDDR3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About self-refresh of DRAM (LPDDR3)

ソリューションへジャンプ
1,513件の閲覧回数
goto11
Contributor III

Hello,

The following is described outside the table of Table 5-5 of the reference manual.
Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?

2.Automatic enter self-refresh when there is no DRAM access.

best regards
Goto

0 件の賞賛
返信
1 解決策
1,504件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi goto11

 

>Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?

 

yes this can be implemented by programming REFRESH_TO_X32 field register DDRC_RFSHCTL0
described in sect.9.2.4.5.2 Refresh using auto refresh feature inside the DDRMC

i.MX 7Dual Applications Processor Reference Manual

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,505件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi goto11

 

>Do I have to set the i.MX7D registers to automatically self-refresh when there is no DRAM access?

 

yes this can be implemented by programming REFRESH_TO_X32 field register DDRC_RFSHCTL0
described in sect.9.2.4.5.2 Refresh using auto refresh feature inside the DDRMC

i.MX 7Dual Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信