About security function with HDMI HDCP1.4 in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About security function with HDMI HDCP1.4 in i.MX6DQ.

1,522件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. My customer got the HDMI HDCP1.4 sample application for L3.0.35.

i.MX6DQ has many encryption algorithms in CAAM (like a DES(64bit), 3DES(128bit), AES(256bit), RC4(128bit)).

What kind of algorithms is use in HDCP1.4 application?

Best Regards,

Keita

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,236件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6 HDMI has own HDCP Encryption Engine. The CAAM is used to

encrypt / decrypt keys, stored in i.MX6 OTP. Please refer to "Android HDCP2.x
User's Guide" of Android documentation.

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.1.0_ANDROID_DOCS&Parent_nodeId=133769948107... 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,236件の閲覧回数
keitanagashima
Senior Contributor I

Hi Yuri,

Thank you for your prompt reply.

Sorry. I update my question.

[Question]

> The i.MX6 HDMI has own HDCP Encryption Engine.

What type of algorithm is used in this HDCP Encryption Engine in HDMI block? (Dedicated algorithm for HDCP1.4? AES? DES?)

I think that 56 bit dedicated algorithm for HDCP1.4.

Best Regards,

Keita

0 件の賞賛
返信

1,236件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello, Keita !

   yes - 56-bit encryption scheme is used for HDCP 1.4

Regards,

Yuri.

0 件の賞賛
返信