About secure boot KPI keys

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About secure boot KPI keys

跳至解决方案
2,149 次查看
changbaoma
Contributor IV

When generate KPI keys tree used in secure boot by hab4_pki_tree.sh.

What is the maximum years of the PKI tree keys duration?

What would happen if this max duration is expired?

0 项奖励
回复
1 解答
2,107 次查看
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.

在原帖中查看解决方案

5 回复数
2,130 次查看
changbaoma
Contributor IV

Hi, Yuri

I have read your post above, but also confuse me.

What is the maximum duration can i set? 10 years?  or 1000 years? or more?

If the KPI keys are valid for 10 years, can the current generated KPI keys be used to sign a new image after 10 years?  Or i must to generated new KPI keys at that time.

0 项奖励
回复
2,124 次查看
Yuri
NXP Employee
NXP Employee

Use 10 year - no need to modify the keys after this period.

 

~Yuri.

0 项奖励
回复
2,121 次查看
changbaoma
Contributor IV

Our customs may use our products 50 years,even 200 years. 

During this period, we need to do equipment maintenance all the time, and will still upgrade and re-sign zImage.

can we input 200 (years) even 1000 years? @Yuri 

0 项奖励
回复
2,108 次查看
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.