About "MCIMX7D-SABRE"

cancel
Showing results for 
Search instead for 
Did you mean: 

About "MCIMX7D-SABRE"

Jump to solution
286 Views
okamotosatoshi
Contributor IV

Hi There,

I want to check for "MCIMX7D-SABRE Rev.D".

MCIMX7D-SABRE is connected to the PMIC_PWR to VLDO34IN.
PMIC_PWR is 3.7V supply power.

PMIC data sheet has the following description.
 Document Number: PF3000 Rev. 7.0, 9/2016

Absolute maximum ratings of VLDO34IN is "-0.3 to 3.6V"
This will be the fact that in violation of the spec.

Is this the SABRE board right connection ?

Best regards
 - satoshi

Labels (3)
0 Kudos
1 Solution
103 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Satoshi

 

recommended to follow latest pmic datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf 

 

Best regards
igor

View solution in original post

0 Kudos
3 Replies
103 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Satoshi

seems pmic specs were finally defined after board was designed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
103 Views
okamotosatoshi
Contributor IV

Hi, igor

Thank you for your reply.

There is a power map in the PMIC data sheet.
Figure 5.  PF3000 typical power map
Here, VIN is connected as a power source of VLDO3 / VLDO4.

(VIN is typical 4.5V?)

VLDO34IN is Will voltage range of 2.8-3.6V is correct?

However, VLDO1 is 2.8-4.5V becomes the input power supply in the same configuration.

Best regards
 - satoshi

0 Kudos
104 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Satoshi

 

recommended to follow latest pmic datasheet

http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf 

 

Best regards
igor

View solution in original post

0 Kudos