Hello, community
I do not use USB Host function,so USB_H1_DP(E10) and USB_H1_DN(F10) will be left not be connected.
Should I just left it not connected or should I connect it to ground or connect it to 3.3V.
Thank you!
ZongbiaoLiao
Solved! Go to Solution.
Hello,
The recommended connections for unused analog interfaces can be found in the section,
“Unused analog interfaces,” of the Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite,
6Solo Families of Applications Processors (IMX6DQ6SDLHDG).
http://cache.nxp.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
In particular, USB_H1_DN, USB_H1_DP, USB_H1_VBUS, USB_OTG_CHD_B,
USB_OTG_DN, USB_OTG_DP, USB_OTG_VBUS may be left float.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The recommended connections for unused analog interfaces can be found in the section,
“Unused analog interfaces,” of the Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite,
6Solo Families of Applications Processors (IMX6DQ6SDLHDG).
http://cache.nxp.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
In particular, USB_H1_DN, USB_H1_DP, USB_H1_VBUS, USB_OTG_CHD_B,
USB_OTG_DN, USB_OTG_DP, USB_OTG_VBUS may be left float.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------