About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

跳至解决方案
1,385 次查看
yuuki
Senior Contributor II

Dear all,

We were estimating KK4.4.2 on the SABRE-SD board.

AndroidKK4.4.3 was released on the Web site of Freescale, so we're trying that.

However, the file configuration of the Bootloader is changed from KK4.4.2.

Could you teach the file doing parameter setting of DDR and PHY?
(File name and location)

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 解答
1,274 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,275 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,274 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

Android KK4.4.3 is based on Linux 3.10.53 kernel,

in kernels with device tree dcd data (setting of DDR) is defined in file

ubootxx/board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,274 次查看
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

We were able to find a file for mx6dl and mx6solo.
However, we were not able to find a file for mx6quad.

Do we have to make a file for mx6quad?

Best Regards,
Yuuki

0 项奖励
回复
1,274 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复