About package installation of glid2 for LTIB of MX6LinuxBSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About package installation of glid2 for LTIB of MX6LinuxBSP

ソリューションへジャンプ
2,455件の閲覧回数
yuuki
Senior Contributor II

About package installation of glid2 for LTIB of MX6LinuxBSP

Environment is the following.
- MCIMX6DL-SDP
- L3.0.35_4.1.0_ER_SOURCE_BSP

We would like to incorporate gstreamer.


However, the following error occurs.

"import is needed by glib2-2.22.1-1"

Would you teach the method for solving this error?

Beset Regards,

ラベル(3)
0 件の賞賛
返信
1 解決策
2,127件の閲覧回数
JackLee1z
NXP Employee
NXP Employee

Hi Yuuki,

When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?

BR,

Jack

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,127件の閲覧回数
YixingKong
Senior Contributor IV

Yuuki

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信
2,127件の閲覧回数
carl_wei
Contributor I

Hi yuuki, do  you have solved  this error ?  when I build Qt by ltib , the same error occurs:

Processing: glib2

===================

sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' glib2 2>/dev/null

sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/Carl/LTIB/ltib/rpm/RPMS/arm/glib2-2.22.1-1.arm.rpm

error: failed dependencies:

    import   is needed by glib2-2.22.1-1

BSP:

L3.0.35_4.1.0_ER_SOURCE_BSP

2,127件の閲覧回数
yuuki
Senior Contributor II

Dear Carl Wei-san,

Thank you for the comment.

This problem has not been solved yet.
I am waiting for the reply from Freescale.

0 件の賞賛
返信
2,127件の閲覧回数
YixingKong
Senior Contributor IV

Yuuki

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
2,128件の閲覧回数
JackLee1z
NXP Employee
NXP Employee

Hi Yuuki,

When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?

BR,

Jack

0 件の賞賛
返信