About overcurrent of SoC line that occurs when the power is turned on i.MX6D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About overcurrent of SoC line that occurs when the power is turned on i.MX6D

9,174 次查看
takashitakahash
Contributor III

Dear community.

Our customer has question below.

the following power supply configuration, over-current flows in the SoC of the line before and after the oscillation of the GDC, SoC power supply voltage is reduced in its influence.

Events subsequent power resulting in OFF has occurred.

Waveform of when an event occurs Please refer to the attachment sheet.

For this reason would you please advice.

- ARM / SoC after the power is turned on, the reason for that the movement and the mechanism by which the over-

  current is generated before and after the GDC is to start the oscillation is the correct design.

- Workaround at GDC side order, this event will not happen.

please refer attachment figure.

Thanks,

Best.

标签 (1)
0 项奖励
回复
7 回复数

8,835 次查看
takashitakahash
Contributor III

Dear Artur.

Vender is ROHM.

The model name is BD90521EFV-C.

Thank you ,

Best Regards.

T.Takahashi

0 项奖励
回复

8,835 次查看
art
NXP Employee
NXP Employee

As specified in the part's Data Sheet document I've found on the part vendor's web site:

http://rohmfs.rohm.com/en/products/databook/datasheet/ic/power/switching_regulator/bd90521xxx-c-e.pd...

the maximum output current the part can supply is 2.0A. On the other hand, the Data Sheet document for the i.MX6Dual/Quad processors specifies that, in some conditions (especially, at power-up or running highly resource-consuming applications), the current consumption on the VDD_ARM_IN and VDD_SOC_IN power rails can exceed 2.0A. So, I suggest you to use the power supply parts that can provide more than 2.0A of output current (at least 2.5A for i.MX6Dual processor) as the VDD_ARM_IN and VDD_SOC_IN power supplies.

Best Regards,

Artur

0 项奖励
回复

8,834 次查看
takashitakahash
Contributor III

Thank you for your replay.

1, I attached complete power supply schematic.

2,There are occuer power-on ramp-up only.

Thank you,

Best

0 项奖励
回复

8,833 次查看
art
NXP Employee
NXP Employee

Please specify the part numbers for the VDD_ARM (IC2101) and VDD_SOC (IC2151) power supply ICs.

Artur

0 项奖励
回复

8,833 次查看
art
NXP Employee
NXP Employee

Unfortunately, the information you've provided is not enough to make any consideration on the issue. To make me able to do this, please provide the complete schematics of your system. Also, please specify the maximum measured peak current on the VDD_SOC_IN power rail when the issue occurs.


Have a great day,
Artur

0 项奖励
回复

8,833 次查看
takashitakahash
Contributor III

Dear Artur-san.

@

Thank you for your replay.

I attach the maximum current measurement results and the circuit diagram.

Would you please be analyzed.

Thank you,

Best.

0 项奖励
回复

8,833 次查看
art
NXP Employee
NXP Employee

1. The schematic you've provided is incomplete, the power supply is not shown there. Please provide the complete schematic.

2. When do these current peaks occur? Do they occur in a random moments, or during initial VDD_SOC_IN voltage power-on ramp-up only? Please clarify.

Artur

0 项奖励
回复