About output between VDD_PU and VDD_SOC LDO in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About output between VDD_PU and VDD_SOC LDO in i.MX6DQ.

Jump to solution
655 Views
keitanagashima
Senior Contributor I

Dear All,

Refer to the Note of Table 6. Operating Ranges in IMX6DQAEC(Rev.4).

======

6  VDD_SOC_CAP and VDD_PU_CAP must be equal.

7  VDD_SOC LDO output set point is equal to the VDD_PU LDO output set point.

======

But, VDD_PU LDO is off in uboot or DVFS processing with VDD_SOC LDO enabled in jb4.2.2_1.1.0.

Does this have the possibility to cause a problem?

(Some issue wasn't seen on custom board.)

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
392 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

these restrictions are only applicable for case when VDD_PU LDO is on.

Best regards

igor
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
393 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

these restrictions are only applicable for case when VDD_PU LDO is on.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos