About maximum density of NAND Flash for GPMI of i.MX8MMini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About maximum density of NAND Flash for GPMI of i.MX8MMini

ソリューションへジャンプ
685件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

We want to connect NAND Flash to GPMI of i.MX8MMini.
We want to know the maximum density that can connect with one CS.

 

I guess it's same as i.MX6 so there are no limitations because of following thread.

https://community.nxp.com/message/523513 

May I have advice?

 

Ko-hey

ラベル(1)
0 件の賞賛
1 解決策
593件の閲覧回数
b36401
NXP Employee
NXP Employee

Do you mean capacity?
There are no special limitations to NAND Flash density as well.

元の投稿で解決策を見る

0 件の賞賛
1 返信
594件の閲覧回数
b36401
NXP Employee
NXP Employee

Do you mean capacity?
There are no special limitations to NAND Flash density as well.

0 件の賞賛