About maximum density of NAND Flash for GPMI of i.MX8MMini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About maximum density of NAND Flash for GPMI of i.MX8MMini

Jump to solution
698 Views
ko-hey
Senior Contributor II

Hi all,

We want to connect NAND Flash to GPMI of i.MX8MMini.
We want to know the maximum density that can connect with one CS.

 

I guess it's same as i.MX6 so there are no limitations because of following thread.

https://community.nxp.com/message/523513 

May I have advice?

 

Ko-hey

Labels (1)
0 Kudos
1 Solution
606 Views
b36401
NXP Employee
NXP Employee

Do you mean capacity?
There are no special limitations to NAND Flash density as well.

View solution in original post

0 Kudos
1 Reply
607 Views
b36401
NXP Employee
NXP Employee

Do you mean capacity?
There are no special limitations to NAND Flash density as well.

0 Kudos