About maximum density of NAND Flash for GPMI of i.MX6Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About maximum density of NAND Flash for GPMI of i.MX6Solo

ソリューションへジャンプ
600件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We want to connect NAND Flash to GPMI of i.MX6Solo.
We want to know the maximum density that can connect with one CS.

May I have advice?

Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
526件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

from i.MX6 hardware point of view there is no limitation

on maximum density.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
527件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

from i.MX6 hardware point of view there is no limitation

on maximum density.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛