About maximum density of NAND Flash for GPMI of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About maximum density of NAND Flash for GPMI of i.MX6Solo

Jump to solution
601 Views
yuuki
Senior Contributor II

Dear all,

We want to connect NAND Flash to GPMI of i.MX6Solo.
We want to know the maximum density that can connect with one CS.

May I have advice?

Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
1 Solution
527 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

from i.MX6 hardware point of view there is no limitation

on maximum density.

Best regards

igor
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
528 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

from i.MX6 hardware point of view there is no limitation

on maximum density.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos