Hello,community
About the following three questions
About IRQ56 to IRQ63 in Table 7-1 of i.MX 7Dual Applications Processor Reference ManualI want to know the register names for enabling / disabling INT7 to INT0?
GPIO1 Combined interrupt indication for GPIO1 signal 0 throughout 15
Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?
Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?
Best Regards,
Goto
已解决! 转到解答。
Hi Goto
for enabling / disabling gpio interrupts one can check GPIOx_ICR,
GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)
i.MX 7Dual Applications Processor Reference Manual
>Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?
yes
>Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?
for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)
through GPIO1(15) has enabled interrupt.
"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Goto
for enabling / disabling gpio interrupts one can check GPIOx_ICR,
GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)
i.MX 7Dual Applications Processor Reference Manual
>Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?
yes
>Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?
for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)
through GPIO1(15) has enabled interrupt.
"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------