About imx6ul vf610 adc driver's continuous sampling mode can not enable two channels at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx6ul vf610 adc driver's continuous sampling mode can not enable two channels at the same time

1,114 Views
kdaadfdafd
Contributor I

The continuous conversion mode of the adc drive can only enable one channel at one time. For example: echo 1 > in_voltage0_en, then echo 1 > in_voltage1_en , prompt echo: write error: Invalid argument. When voltage0 is turned off, voltage1 can be enabled, as shown in the figure below.

{197PHKJILASG1(5DN~2HWV.png
Labels (1)
0 Kudos
Reply
1 Reply

975 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello

The issue it is related to the ADC HW, this ADC Module has only one ADC so the Channels are muxed to input the ADC, this means if you are using the continuos mode only One Channel can be Muxed.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply