About imx6dl hdmi cec and hpd(hotplug detection) question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx6dl hdmi cec and hpd(hotplug detection) question

Jump to solution
1,623 Views
yenchao
Contributor IV

Hi All,

I'm working on imx6dl android 5.1(kernel 3.14.52) and have a question on hdmi cec and hpd(hotplug detection).

That is when a monitor send hpd(hotplug detection) low to our board.

Our board won't receive any hdmi cec signal until we re-initilaize hdmi cec function.

I know it is reasonable for not receiving hdmi cec signal when board receive hpd low.
But I am curious to know why this happen?

Is there any register that will disable hdmi cec signal when board receive hpd low?

Any thoughts or suggestions will be greatly appreciated.

Thx

Yen

Labels (4)
0 Kudos
Reply
1 Solution
1,317 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yen

one can check sect.33.5.219 PHY RXSENSE, PLL lock, and HPD Status Register
(HDMI_PHY_STAT0), sect.33.5.221 PHY RXSENSE, PLL lock, and HPD Mask Register
(HDMI_PHY_MASK0) i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,318 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yen

one can check sect.33.5.219 PHY RXSENSE, PLL lock, and HPD Status Register
(HDMI_PHY_STAT0), sect.33.5.221 PHY RXSENSE, PLL lock, and HPD Mask Register
(HDMI_PHY_MASK0) i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply