About imx6 spi be used on application layer.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About imx6 spi be used on application layer.

ソリューションへジャンプ
1,309件の閲覧回数
guanliangding
Contributor III

Hi, all:

     I config the devicetree and menuconfig like attach. But in the /dev, i don't find spidevx.x still. I use linux kernel is 3.10.17.

clipboard.png

clipboard1.png

clipboard11.png

clipboard111.png

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,030件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,031件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信