About imx6 spi be used on application layer.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About imx6 spi be used on application layer.

跳至解决方案
1,411 次查看
guanliangding
Contributor III

Hi, all:

     I config the devicetree and menuconfig like attach. But in the /dev, i don't find spidevx.x still. I use linux kernel is 3.10.17.

clipboard.png

clipboard1.png

clipboard11.png

clipboard111.png

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,132 次查看
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,133 次查看
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复