About imx6 spi be used on application layer.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx6 spi be used on application layer.

Jump to solution
1,324 Views
guanliangding
Contributor III

Hi, all:

     I config the devicetree and menuconfig like attach. But in the /dev, i don't find spidevx.x still. I use linux kernel is 3.10.17.

clipboard.png

clipboard1.png

clipboard11.png

clipboard111.png

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,045 Views
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,046 Views
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

compatible = "spidev" should be added as in

SPI block device

How to enable and test SPI in i.MX6SoloLite using kernel 3.10.17?

and enable spidev support in the kernel with menuconfig

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply