About imx6 I2S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx6 I2S

648 Views
宗標廖
Contributor V

Hello,Community

I want to use I2S of imx6 as bellow:

imx6 receives data via RX of I2S-X(X:1 or 2 or 3) from peripheral device ,While it is transmitting data via TX of I2S-X.

I don't know whether my idea is right or not.

Could you help me?

Thank you!

Best Regards,

ZongbiaoLiao

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

476 Views
art
NXP Employee
NXP Employee

Of course, you can simultaneously receive data through RX pin and transmit data through TX pin of the same SSI module in I2S mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------