Hello,
I have a question about the contents of i.MX 8M Mini Applications Processor Reference Manual.
Q1: I want to set PMS_P PMS_M PMS_S in MIPI_DPHY_M_PLLPMS (Chapter 13.7.10.1),but I don't know his real address.I noticed that the address in the manual is 0x0000000. [p1.png]
And, I also want to know, for example, my screen resolution is 1024*600, then how do I determine my pms value?
Q2: I want to read the value of SSCG_EN in MIPI_DPHY_M_PLLCTL (Chapter 13.7.10.2). Similarly, I cannot know his address. So, how should I convert between the memory map and the address?
Or how to read the value in MIPI_DPHY_M_PLLCTL? [p2.png]
Q3: Following the last question, I found a description of memory map in the IMX8MMRM manual, which describes that the base address of DISPLAY_BLK_CTRL is 32E2_8000h (Chapter 13.2), and the corresponding GPR_MIPI_M_PLLCTL_LOW address is 32E28010H, so is this the same as the above MIPI_DPHY_M_PLLCTL? [p3.png]
Hope you can help me.
Thanks.