About i.MX7D ibis files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX7D ibis files

Jump to solution
599 Views
goto11
Contributor III

hello,Community


About the mx7d_12x12_1p8v_lpddr3.ibs file
I confirmed that there is a drive strength selection signal such as “PBLPDDR3_DDS_240ohm“ drv000 ”” in the LPDDR3 selection signal.
However, there is no On-die-termination (ODT) resistor value selection signal.
What should I refer to?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
532 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  use chapter 6 (IBIS model)  of the Development Guide.

   http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf 

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
1 Reply
533 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  use chapter 6 (IBIS model)  of the Development Guide.

   http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf 

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply