About i.MX6Solo DDR3 sdclk wiring lengs.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX6Solo DDR3 sdclk wiring lengs.

Jump to solution
649 Views
takashitakahash
Contributor III

Dear community.

Our customer has question below.

The wiring length of DRAM_SDCLK [1: 0] is described as max 2.25 inch,
When DDR 3 branches into two, the wiring length becomes A + C in the case of DDR 3 _a, A + B in the case of DDR _ b,
Do I have to meet  A + C <2.25 inch and A + B <2.25 inch respectively?

Or will it be 2.25 inches including the other branches? (A + B + C <2.25 inch)?

pastedImage_1.png

pastedImage_2.png

Labels (1)
0 Kudos
1 Solution
567 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is necessary to meet  A + C <2.25 inch and A + B <2.25 inch respectively.

Best regards
igor
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
568 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is necessary to meet  A + C <2.25 inch and A + B <2.25 inch respectively.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos