Dear All,
Hello.
I have questions about i.MX6Q in deep sleep mode.
Refer to Table 10-1. Aimed power modes in IMX6DQRM(Rev.2).
There is below description.
"Interrupts from modules those could generate asynchronous interrupts (Keypad, GPIO, SNVS)".
[Q1]
Can i.MX6 return (resume) from deep sleep mode by detection of VBUS with USB?
[Q2]
When entering a sleep-mode, does it make LAN PHY a sleep-mode, too?
(I consider that LAN PHY enters a sleep-mode because the current consumption of LAN_PHY decreased in Sleep Mode.)
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
1. yes
2. yes if used LAN PHY supports such sleep-mode, this may depend
on PHY chip.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
1. yes
2. yes if used LAN PHY supports such sleep-mode, this may depend
on PHY chip.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply.
I tried to test by below command with L3.14.28_1.0.0.
====
echo enabled > /sys/bus/platform/devices/20c9000.usbphy/power/wakeup
echo enabled > /sys/bus/platform/devices/2184000.usb/power/wakeup
echo enabled > /sys/bus/platform/devices/ci_hdrc.0/power/wakeup
echo enabled > /sys/bus/usb/devices/usb1/power/wakeup
====
And, I confirmed USB wake up.
Thank you!
Best Regards,
Keita