About i.MX6Q interrupt priority

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About i.MX6Q interrupt priority

1,739 次查看
ainolike
Contributor III

Dear all,

Hello.

I have a question about interrupt priority in i.MX6Q.

In IMX6DQRM, chapter 2, table2-1 system memory map it gives us the interrupt controller and interrupt distributor registers' address range, but I cannot find the definition about these registers.

Similarly it only gives us the registers’ address about interrupt priority in BSP, besides there is no useful information to this question.

[Q1]

I wonder how to config interrupt priority.

Best regards.

标签 (2)
0 项奖励
回复
2 回复数

1,458 次查看
igorpadykov
NXP Employee
NXP Employee

Hi li

this is described in GIC Architecture Specification from ARM (www.arm.com)

or look at attached document from SDK Chapter 4 Configuring the GIC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,458 次查看
ainolike
Contributor III

Hi

Thanks for your help. I have looked at the document, but I still cannot deal with it.

In the file vxbArmGenIntCtrl.c, it gives some information as follows,

"

Optinally, the interrupt priority and sensitivity can be set as below in hwconf:

\cs

LOCAL const struct intrCtlrPriority armGICPriority[] = {

    { INT_PIN_TIMER,       INT_PRI_TIMER_0},

    { INT_PIN_UART,        INT_PRI_UART_1 },

    { INT_PIN_DMA,         INT_PRI_SDMA   },

    { INT_PIN_END,         INT_PRI_FEC    },

};

\ce

"

Also in BSP of imx31,imx35,imx51,imx53, ect, this method has been used. I try to add my own code in hwconf.c like this.

"

struct intrCtlrPriority imx6Priority[] =

    {

    /* pin,                       priority */

    {IMX_INT_GPIO1,        15},

    {IMX_INT_GPIO2,        1},

    };

const struct hcfResource imx6IntCtlrResources[] =

    {

    { "regBase",           HCF_RES_INT,   {(void *)ARM_GIC_BASE}},

    { "intMode",           HCF_RES_INT,   {(void *)INT_MODE}},

    { "input",             HCF_RES_ADDR,  {(void *)&armGicInputs[0]}},

    { "inputTableSize",    HCF_RES_INT,   {(void *)NELEMENTS(armGicInputs)}},

    { "priority",          HCF_RES_ADDR,  {(void *)&imx6Priority[0]}},

    { "priorityTableSize", HCF_RES_INT,   {(void *)NELEMENTS(imx6Priority)}},

    };

#define imx6IntCtlrNum NELEMENTS(imx6IntCtlrResources)

const struct hcfDevice hcfDeviceList[] = {

  {"vxbImx6IntCtrl",      0, VXB_BUSID_PLB,   0,  imx6IntCtlrNum,     imx6IntCtlrResources},

...

"

But it I could get what i want. Could I do like this? And where is my problem?

0 项奖励
回复