About i.MX53 ENGcm11133.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX53 ENGcm11133.

Jump to solution
545 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX53 ENGcm11133.

Please see "Description" of ENGcm11133 in IMX53CE (Rev.5).

Our partner want to confirm the condition to occur this errata.

The conditions are as follows:

=====

• Neon loads and stores must be in use

• Neon L1 caching must be disabled

• Trustzone must be configured and in use

• The secure memory address space and the non-secure memory address space both use the same

physical addresses, either as an alias or the same memory location or for separate memory locations

=====

We understand this errata is occurred when all the above condition is satisfied, right?

Or it is occurred when any one of the above condition is satisfied?

Best Regards,

Satoshi Shimoda

Labels (1)
0 Kudos
Reply
1 Solution
514 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, you are right, it will happen when all conditions are satisfied.

View solution in original post

0 Kudos
Reply
1 Reply
515 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, you are right, it will happen when all conditions are satisfied.

0 Kudos
Reply