About glTexDirectVIVMap() in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About glTexDirectVIVMap() in i.MX6DQ.

Jump to solution
3,538 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

When transferring an image to the texture which was created by using glTexDirectVIV(), DMA can transfer it by using glTexDirectVIVMap().

When using a texture and rendering a polygon, the contents of the texture are always updated (i.e.using DMA transfer), in case of calling glTexDirectVIVMap() and DMA transfer's being set.

(When setting a camera image by the DMA transfer in glTexDirectVIVMap(), after that, the contents of the texture are always updated.)

[Question]

Is there a way of not making always update the contents of the texture?

BSP : L3.14.28_1.0.0

Best Regards,

Keita

Labels (4)
0 Kudos
Reply
1 Solution
1,788 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

Are you using glTexDirectInvalidateVIV ?

glTexDirectVIV() − Driver reserves memory for texture, and return pointer

glTexDirectVIVMap() − User reserves logical (and physical) continuous memory, then driver map the memory as a texture memory.

glTexDirectInvalidateVIV() − Tell GPU texture memory is updated

One example could be:

First, call glTexDirectVIV to get a pointer.

Second, copy the texture data to this memory address

Then, call glTexDirectInvalidateVIV to apply the texture before you draw something with that texture

Hope this helps

View solution in original post

0 Kudos
Reply
2 Replies
1,789 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

Are you using glTexDirectInvalidateVIV ?

glTexDirectVIV() − Driver reserves memory for texture, and return pointer

glTexDirectVIVMap() − User reserves logical (and physical) continuous memory, then driver map the memory as a texture memory.

glTexDirectInvalidateVIV() − Tell GPU texture memory is updated

One example could be:

First, call glTexDirectVIV to get a pointer.

Second, copy the texture data to this memory address

Then, call glTexDirectInvalidateVIV to apply the texture before you draw something with that texture

Hope this helps

0 Kudos
Reply
1,788 Views
philbot999
Contributor I

Hi All,

This thread seems to discuss exactly what I want to accomplish - direct V4L2 video buffers to OpenGL Textures via DMA.

Is there any simple, yet complete, example application in the imx BSP?

Thank you very much,

Phil

0 Kudos
Reply