I use freescale' Quick Stard Board mounting i.mx535 processor ( Full P/N = PCIMX535DVV1C)
I boot Quick Stard Board with given pre-built image in SD card.
Next, I excute example program in the next path.
/home/lucid/Desktop/gpu-sdk1008/bin/ es2_lesson02_fbdev
then error message printed at console is next <table1>.
<table 1>
=========================================================================
lucid@lucid-desktop:~/Desktop/gpu-sdk1008/bin$ ./es2_lesson02_fbdev
es2_lesson02_fbdev: lesson02_imx.c:231: int init(): Assertion `eglGetError() == 0x3000' failed.
Aborted
=========================================================================
Then. I edit /etc/init/rc-sysinit.conf in root filesystem same as following sentence.
=========================================================================
*. Before change : env DEFAULT_RUNLEVEL=2
*. After change : env DEFAULT_RUNLEVEL=1
=========================================================================
Then, I boot Quick Stard Board.
then, I excute the example program(=es2_lesson02_fbdev) in the same path.
then, error message same as <table1> is printed.
Please.
What is the problem ?
Please help me…!!!
Thank you very much.
Oh, wait. Found that if I grab the libraries and bins from amd-gpu-mx51 in the patch bundle from the website I get framebuffer support. This is distinct from the amd-gpu-x11-mx51 libs and bins. The libs have the same name so I might put them in a different location and use LD_LIBRARY_PATH depending if I want X11 or fbdev.
I have the same issue with a imx53 QSB-R and the default image. The es1, es2 and vg demos all fail to initialise using the _fbdev version in gpu-sdk1008. This issue is mentioned elsewhere in the forums but I have not seen any response. Is this a known problem and is there a resolution?