About dropout of LSCLK of i.MX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About dropout of LSCLK of i.MX25

ソリューションへジャンプ
1,671件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We connect an LCD panel to i.MX25.
We observed a waveform of OE and LSCLK.

When OE signal changes in High, LSCLK drops out 1clk.
(It occurs in every rising of the OE signal.)
Please see the following figure.

LSCLK_OE.png

We investigate this cause.
May I have any advice?

Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,578件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

plaese check TLSbo95476 LCDC: LSCLK is missing

IMX25CE Chip Errata for the i.MX25

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,579件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

plaese check TLSbo95476 LCDC: LSCLK is missing

IMX25CE Chip Errata for the i.MX25

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信