About difference in memory reading speed by the Android version for i.MX6 Quad.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About difference in memory reading speed by the Android version for i.MX6 Quad.

1,294 次查看
yuuki
Senior Contributor II

Dear all,

We run Android BSP on MX6Quad SABRE-SDB board.

We noticed that memory reading speed was different between Android4 .4.2 and Android4 .4.3.

<Measurement result>
* Android4.4.2
    eMMC Seq.Read=47.49MB/s,   SD Seq Read=22.69MB/s

* Android4.4.3
    eMMC Seq.Read=35.38MB/s,   SD Seq Read=17.92MB/s

Would you tell me the factor of the difference in this speed?

May I have any advice?

Best Regards,
Yuuki Murasato

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,189 次查看
b36401
NXP Employee
NXP Employee

Are you using the same way to measure the speed?

Please make sure that the board is running with the same clocks.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,189 次查看
yuuki
Senior Contributor II

Dear Victor-san,

I am sorry to delay.

Thank you for your support.

We measured by the same method.
The clock setting for eMMC/SD is the same, too.
The write speed is almost similar.

However, we seem that a performance of the reading speed may be inferior in Android4.4.3.

Are there any patches for eMMC/SD I/F in Android4.4.3?

Best Regards,
Yuuki

0 项奖励
回复