About /dev/mmcblk3rpmb operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About /dev/mmcblk3rpmb operation

1,824 Views
jason_rsmgnu
Contributor II

How Can I operate the eMMC RPMB partition?  When I mount this patition,the information is below:

root@imx6qsabresd:/dev# mount /dev/mmcblk3rpmb /mnt/
[ 458.812486] EXT4-fs (mmcblk3rpmb): unable to read superblock
[ 458.818792] EXT3-fs (mmcblk3rpmb): error: unable to read superblock
[ 458.825612] EXT2-fs (mmcblk3rpmb): error: unable to read superblock
[ 458.832345] FAT-fs (mmcblk3rpmb): unable to read boot sector
[ 458.847143] EXT3-fs (mmcblk3rpmb): error: unable to read superblock
[ 458.853665] EXT2-fs (mmcblk3rpmb): error: unable to read superblock
[ 458.860122] EXT4-fs (mmcblk3rpmb): unable to read superblock
[ 458.865996] FAT-fs (mmcblk3rpmb): unable to read boot sector
mount: mounting /dev/mmcblk3rpmb on /mnt/ failed: Invalid argument
root@imx6qsabresd:/dev# @

Tags (1)
0 Kudos
Reply
1 Reply

1,270 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try using mmc-utils for RPMB operations.

Boot from eMMC mmcblk3boot0 or mmcblk3boot1. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply