About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

跳至解决方案
1,406 次查看
yuuki
Senior Contributor II

Dear all,

I am referring to IOMUXC_GPR1 register.

IMX6SDLRM.pdf (Rev1)
- IOMUXC_GPR1 field descriptions(P.2033)

For 19-20 filed and bit13, these field names are indicated as "-".

Are these Reserved?

If these are not Reserved,
Would you teach the details of 19-20 field?


Best Regards,

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,179 次查看
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,180 次查看
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复