About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

Jump to solution
1,433 Views
yuuki
Senior Contributor II

Dear all,

I am referring to IOMUXC_GPR1 register.

IMX6SDLRM.pdf (Rev1)
- IOMUXC_GPR1 field descriptions(P.2033)

For 19-20 filed and bit13, these field names are indicated as "-".

Are these Reserved?

If these are not Reserved,
Would you teach the details of 19-20 field?


Best Regards,

Labels (1)
0 Kudos
Reply
1 Solution
1,206 Views
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,207 Views
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply