About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About description of 19-20 filed and bit13 of IOMUXC_GPR1 field of i.MX6DL

ソリューションへジャンプ
1,405件の閲覧回数
yuuki
Senior Contributor II

Dear all,

I am referring to IOMUXC_GPR1 register.

IMX6SDLRM.pdf (Rev1)
- IOMUXC_GPR1 field descriptions(P.2033)

For 19-20 filed and bit13, these field names are indicated as "-".

Are these Reserved?

If these are not Reserved,
Would you teach the details of 19-20 field?


Best Regards,

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,178件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,179件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The mentioned bits of the GPR1 are not used in i.MX6 S/DL devices,

they are intended for i.MX6 D/Q parts.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信