About connection of SPI-NOR Flash in i.MX6D.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About connection of SPI-NOR Flash in i.MX6D.

ソリューションへジャンプ
1,899件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about connection of SPI-NOR Flash in i.MX6D.

[Q1]

Tell me the maximum capacity of SPI-NOR which it is possible to connect with i.MX6D.

[Q2]

(See attached file: SPI-NOR_connection.PNG)

Is it possible to connect like an attached file?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,678件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.
  The main size restriction of SPI NOR relates to boot mode : from section 8.5.5.3 (ECSPI Boot) of i.MX6 DQ RM :
"The ECSPI can read data from EEPROM using 2 or 3 byte addressing". So, boot mode is supported up to 16M. 


2.
   Several SPI NOR devices may be connected to i.MX6, since we have four Chip Select (SS) signals per CSPI
controller (ECSPIx_SSy), and five ECSPI modules. But only single channel may be used for boot.

Note, QSPI is not supported by i.MX6. Also HOLD signal is not used in i.MX6 ECSPI. It may be recommended
just to terminate this signal in inactive state.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,679件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.
  The main size restriction of SPI NOR relates to boot mode : from section 8.5.5.3 (ECSPI Boot) of i.MX6 DQ RM :
"The ECSPI can read data from EEPROM using 2 or 3 byte addressing". So, boot mode is supported up to 16M. 


2.
   Several SPI NOR devices may be connected to i.MX6, since we have four Chip Select (SS) signals per CSPI
controller (ECSPIx_SSy), and five ECSPI modules. But only single channel may be used for boot.

Note, QSPI is not supported by i.MX6. Also HOLD signal is not used in i.MX6 ECSPI. It may be recommended
just to terminate this signal in inactive state.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信