Dear Sir or Madam,
Hello.
I have a question about connection of SPI-NOR Flash in i.MX6D.
[Q1]
Tell me the maximum capacity of SPI-NOR which it is possible to connect with i.MX6D.
[Q2]
(See attached file: SPI-NOR_connection.PNG)
Is it possible to connect like an attached file?
Best Regards,
Keita
Solved! Go to Solution.
1.
The main size restriction of SPI NOR relates to boot mode : from section 8.5.5.3 (ECSPI Boot) of i.MX6 DQ RM :
"The ECSPI can read data from EEPROM using 2 or 3 byte addressing". So, boot mode is supported up to 16M.
2.
Several SPI NOR devices may be connected to i.MX6, since we have four Chip Select (SS) signals per CSPI
controller (ECSPIx_SSy), and five ECSPI modules. But only single channel may be used for boot.
Note, QSPI is not supported by i.MX6. Also HOLD signal is not used in i.MX6 ECSPI. It may be recommended
just to terminate this signal in inactive state.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
1.
The main size restriction of SPI NOR relates to boot mode : from section 8.5.5.3 (ECSPI Boot) of i.MX6 DQ RM :
"The ECSPI can read data from EEPROM using 2 or 3 byte addressing". So, boot mode is supported up to 16M.
2.
Several SPI NOR devices may be connected to i.MX6, since we have four Chip Select (SS) signals per CSPI
controller (ECSPIx_SSy), and five ECSPI modules. But only single channel may be used for boot.
Note, QSPI is not supported by i.MX6. Also HOLD signal is not used in i.MX6 ECSPI. It may be recommended
just to terminate this signal in inactive state.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------