About connection of IMX7 and LPDDR3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About connection of IMX7 and LPDDR3

跳至解决方案
2,261 次查看
okamotosatoshi
Contributor IV

Hi There,

I want to check for IMX7.
I want to connect the IMX7 and LPDDR3.
Do you have a document that describes the pin mapping of LPDDR3 ?

The IMX6, there was pin mapping of LPDDR2.
 Applications Processor Reference Manual -  Multi Mode DDR Controller (MMDC) - LPDDR2 and DRAM pin mux mapping

LPDDR2 and DRAM pin mux mapping.png

Best regards
 - satoshi

标签 (1)
0 项奖励
回复
1 解答
1,873 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复
5 回复数
1,873 次查看
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for your reply.

The meaning of "No special mapping",
Is a document the meaning that there is not ?
or
Should I be connected as well as a document?
http://cache.nxp.com/files/nxp/brochure/WARP7-FLYER-V2.pdf?

Best regards
 - satoshi

0 项奖励
回复
1,874 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复
1,873 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

 

  You may look at the WARP 7 design, where LPDDR3 with i.MX7 are applied.

 

http://cache.nxp.com/files/nxp/brochure/WARP7-FLYER-V2.pdf 

 

Design file for WaRP7 board (Schematics & P... | element14 | Technical Library 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct
Answer button. Thank you!

------------------------------------------------------------------------------

0 项奖励
回复
1,873 次查看
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for information and in reference document.
I will do the reference for circuit design.

I use IMX7 Dual.
 Device:「MCIMX7D7DVM10SC」

Do you have a document that describes the pin mapping of LPDDR3 and IMX7 Dual ?

Best regards
 - satoshi

0 项奖励
回复
1,873 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  No special mapping for LPDDR3 for i.MX7.

Regards,

Yuri.

0 项奖励
回复