About connection of IMX7 and LPDDR3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About connection of IMX7 and LPDDR3

ソリューションへジャンプ
2,262件の閲覧回数
okamotosatoshi
Contributor IV

Hi There,

I want to check for IMX7.
I want to connect the IMX7 and LPDDR3.
Do you have a document that describes the pin mapping of LPDDR3 ?

The IMX6, there was pin mapping of LPDDR2.
 Applications Processor Reference Manual -  Multi Mode DDR Controller (MMDC) - LPDDR2 and DRAM pin mux mapping

LPDDR2 and DRAM pin mux mapping.png

Best regards
 - satoshi

ラベル(1)
0 件の賞賛
返信
1 解決策
1,874件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
5 返答(返信)
1,874件の閲覧回数
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for your reply.

The meaning of "No special mapping",
Is a document the meaning that there is not ?
or
Should I be connected as well as a document?
http://cache.nxp.com/files/nxp/brochure/WARP7-FLYER-V2.pdf?

Best regards
 - satoshi

0 件の賞賛
返信
1,875件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
1,874件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 

  You may look at the WARP 7 design, where LPDDR3 with i.MX7 are applied.

 

http://cache.nxp.com/files/nxp/brochure/WARP7-FLYER-V2.pdf 

 

Design file for WaRP7 board (Schematics & P... | element14 | Technical Library 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct
Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信
1,874件の閲覧回数
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for information and in reference document.
I will do the reference for circuit design.

I use IMX7 Dual.
 Device:「MCIMX7D7DVM10SC」

Do you have a document that describes the pin mapping of LPDDR3 and IMX7 Dual ?

Best regards
 - satoshi

0 件の賞賛
返信
1,874件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  No special mapping for LPDDR3 for i.MX7.

Regards,

Yuri.

0 件の賞賛
返信